M-Bus - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

M-Bus (Meter Bus) is a European standard (EN 13757-3) that applies to heat and electric meters. These meters measure the heat absorbed or released by an energy-conveying liquid in a heat-exchange circuit. An M-Bus level converter is necessary for an M-Bus integration. The converter connects a network engine to an M-Bus network.