Equipment Controllers - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

Metasys includes several model series of equipment controllers, including General Purpose Application Controllers (CG series), VAV Box Controllers (CV series), Advanced Application Field Equipment Controllers (FACs), Field Equipment Controllers (FECs), Variable Air Volume Modular Assembly (VMAs), Input/Output Modules (IOMs), and Expansion Input/Output Modules (XPMs). These devices provide direct, operational control over HVAC and other mechanical and electrical equipment and are typically networked together and supervised by network engines. The BACnet® family of controllers is tested by an independent BACnet Testing Lab. A complete listing of the tested Johnson Controls® BACnet devices is available at the following link: http://www.bacnetinternational.net/btl/index.php?m=15