Expansion input and output (I/O) modules - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active
IOM controllers
The IOM controllers are expansion input and output modules with integral RS-485 MS/TP communications. IOMs can serve in one of two capacities, depending on where they are installed in the Metasys system. When installed on the SA Bus of a CGM, CGE, CVM, CVE, FAC, FEC, or VMA controller, the IOMs expand the point count of these controllers. When installed on the FC Bus, the IOMs support monitoring and control from an NAE or NCE as I/O point multiplexors. The point multiplexor can also be useful for sharing points between other field controllers on the FC Bus using peer-to-peer connectivity. A full range of CGM, CGE, CVM, CVE, FAC, FEC, and VMA models combined with the IOM models can be applied to a wide variety of mechanical and electrical equipment control applications ranging from simple fan coil or heat pump control to advanced central plant management.
M4-XPM series expansion I/O modules

The M4-XPM series input/output (I/O) expansion modules are part of the Metasys system CG, CV Equipment Controller family and can serve in one of two capacities depending on where they are installed in the Metasys system. When installed on the Sensor/Actuator (SA) Bus of a Metasys controller, an XPM expands the input and output interfaces that can be used with that equipment controller. When installed on the Field Controller (FC) Bus of a Metasys network engine, an XPM can be used as I/O point multiplexors to support monitoring and control from a Metasys network engine. The point multiplexor can also be useful for sharing points between other equipment controllers on the FC Bus using peer-to-peer connectivity.

XPMs operate on an RS-485 BACnet MS/TP Bus and are BACnet Testing Laboratory (BTL) listed and certified to the BACnet Smart Actuator (B-SA) profile.

Compatibility:

XPM series expansion modules can be connected to the SA Bus of the following equipment controller device types:
  • CG series General Purpose Application Equipment Controllers
  • CV series VAV Box Controllers
  • FAC series Advanced Application Field Equipment Controllers
  • FEC series Field Equipment Controllers
  • VMA16, VMA17, VMA18, and VMA19 series VAV Box Controllers
  • SNC series Network Control Engines
  • NCE series Network Control Engines
Note: XPM series expansion modules may coexist on the SA Bus with IOM series input/output expansion modules.
XPM series expansion modules can be connected to the FC bus of the following network engine types:
  • SNE series Network Engines
  • SNC series Network Control Engines
  • NAE35, NIE39, NAE45, NAE49, NAE55, and NAE59 series Network Automation and Integration Engines
  • NCE25 and NIE29 series Network Control Engines
Note: XPM series modules may coexist on the FC Bus with IOM series input/output expansion modules.

For more information about the M4-XPM series, refer to the M4-XPM Expansion Modules Catalog Page (LIT-1901145).