Introduction - Metasys - LIT-12013153 - System Integration - Molex Lighting Integration - 11.0

Metasys System Commissioning for Molex Digital Lighting Systems Integration

Product
Integrations > Molex Lighting Integrations > Molex Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013153
Version
11.0
Revision date
2020-10-30

This document describes how to commission a network engine for integration with the Molex® lighting system. In this document, network engine refers to an NAE55, NAE85, SNE, or SNC series network engine, unless noted otherwise.

This document does not describe the following:
  • The commissioning steps required for a server-based NAE85 to operate on a Metasys® Building Automation System (BAS) network. For more information about commissioning an NAE85 software, refer to the NAE85 Commissioning Guide (LIT-12011044).
  • How to mount, wire, or power on an network engine.
  • How to build or download an archive database for a Metasys system site.
  • How to configure an network engine to monitor and control a BAS.

For information about installing network engines, refer to the NAE55 Installation Instructions (Part No. 24-10051-43), NAE35/45 Installation Instructions (Part No. 24-10050-6), NCE25 Installation Instructions (Part No. 24-10143-63), SNC Installation Guide (Part No. 24-10143-01892), or SNE Installation Guide (Part No. 24-10143-01647) . For information about installing NAE85 software, refer to the NxE85 Installation and Upgrade Instructions (LIT-12011530).