Requirements - Metasys - LIT-12013153 - System Integration - Molex Lighting Integration - 11.0

Metasys System Commissioning for Molex Digital Lighting Systems Integration

Product
Integrations > Molex Lighting Integrations > Molex Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013153
Version
11.0
Revision date
2020-10-30

To add a Molex CoreSync integration over BACnet/IP to a network engine, you must have the following:

  • The Molex lighting system must already be working and performing its primary function before you attempt an integration with Metasys. This means the Molex lighting system has been properly installed and commissioned using CoreSync Manager software installed on the Molex server with the Molex BACnet Gateway service running.
  • A properly installed and commissioned Johnson Controls network engine from which to perform the BACnet/IP integration.
  • System Configuration Tool (SCT) Release 14.0