Procedure
-
In the All Items tree, select the network engine for the integration.
-
On the Facility menu, select Rapid Archive. The Rapid
Archive Field Controller wizard appears.
-
Click Edit.
-
Click Import, browse to the location of the Rapid
Archive Schedule .csv file, then click Import.
-
After the import completes, the Import Room Schedule dialog appears. Click
OK.
Figure 1. Rapid Archive Field Controller wizard populated with example lighting
data
-
A cell highlighted in red indicates an error. If there is an error, click
Cancel, modify the Rapid Archive Schedule to correct
the error, and repeat the process from Step 3.
-
Click Save.
-
Refresh the All Items tree to verify that your virtual
lighting devices and points populated correctly.
Figure 2. Imported virtual devices shown in All Items tree