Preparing an equipment definition in SCT - Metasys - LIT-12013153 - System Integration - Molex Lighting Integration - 11.0

Metasys System Commissioning for Molex Digital Lighting Systems Integration

Product
Integrations > Molex Lighting Integrations > Molex Lighting Integration
Document number
LIT-12013153
Version
11.0
Revision date
2020-10-30

About this task

You can download a lighting equipment definition from the Global Library site: https://globallibrary.azurewebsites.net/#/equipmentdefinition. The equipment definition defines a selection of the available points in a lighting virtual device that are presented in the Metasys UI. The equipment definition is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Insert Equipment Definition section in the Metasys SCT Help (LIT-12011964).

Procedure

  1. Download the equipment definition file from Johnson Controls.
  2. Launch the SCT, and then open an archive.
  3. In the All Items tree, expand the server object, for example the ADS or ADX.
  4. Right-click the Equipment Definitions folder, and then click Import Equipment Definition.
  5. Navigate to the location of the equipment definition, select the file, then click Import.
  6. After the import is complete, a confirmation message appears. Click OK. The equipment definition imports and is listed under the Equipment Definitions folder.