Preparing a controller template for lighting in SCT - Metasys - LIT-12013153 - System Integration - Molex Lighting Integration - 11.0

Metasys System Commissioning for Molex Digital Lighting Systems Integration

Product
Integrations > Molex Lighting Integrations > Molex Lighting Integration
Document number
LIT-12013153
Version
11.0
Revision date
2020-10-30

About this task

You can download a lighting controller template from the Global Library site: https://globallibrary.azurewebsites.net/#/controllertemplate. The controller template defines a set of points that are available in a lighting virtual device. The controller template is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Controller Templates section in the Metasys SCT Help (LIT-12011964)

For the list of points included in the controller templates, see Table 1, Table 2, and Table 3.

Table 1. Point list for lighting controller template
Item reference Name Class ID Units States text Description Instance number
BV-11501 Lights on BACnet BV   On/Off Zone light on or off 11501
AV-10001 Lighting level BACnet AV % 0-100 Zone light level 10001
MV-10751 Light scene BACnet MV     Named lighting scenes configured in CoreSync 10751
BI-13751 Space occupied BACnet BI   Unocc / Occ PIR occupancy sensor 13751
AI-13004 Total power usage BACnet AI W   Power consumed by all the lighting devices in a space 13004
AI-13003 Average color temperature BACnet AI K   Zone average color temperature 13003
AI-13001 Ambient light level BACnet AV lx   The average ambient lux value as seen by all sensors in the space 13001
BACnet positive integer value-12251 Ambient light level target BACnet positive integer value lx   Sets the target lux level to use for daylight harvesting 12251
BACnet positive integer value-12252 Occupancy timeout BACnet positive integer value seconds   The length of time the space is unoccupied before the lights begin to fade out 12252
BACnet positive integer value-12253 Occupancy fadeout BACnet positive integer value seconds   Sets the length of time to fade the lights as long as the space remains unoccupied 12253
Table 2. Point list for add-on sensor controller template
Item reference Name Class ID Units States text Description Instance number
AI-13005 Space temperature BACnet AI °F   The average space temperature as measured by all sensors in the space 13005
AI-13006 Humidity BACnet AI %   The average space humidity as measured by all sensors in the space 13006
AI-13002 Air quality BACnet AI     The average air quality reading as measured by all sensors in the space 13002
Table 3. Point list for beacons controller template
Item reference Name Class ID Units States text Description Instance number
BV-11501 Lights on BACnet BV   On/Off Beacons on or off in the space 11501
AV-10001 Lighting level BACnet AV % 0-100 The brightness of the beacons 10001
BACnet positive integer value-12626 Lighting color BACnet positive integer value     The RGB color of the beacon 12626

To import the controller template into an SCT archive, complete the following steps:

Procedure

  1. Download the controller template file from Johnson Controls.
  2. Launch the SCT, and then open an archive.
  3. In the All Items tree, expand the Configuration Data folder.
  4. Right-click the SCT Controller Templates folder, and then click Import Template.
  5. Navigate to the location of the controller template, select the template, then click Import.
  6. After the import is complete, a confirmation message appears. Click OK. The controller template imports and is listed under the SCT Controller Templates folder.

Results