Linking a controller template to an equipment definition in SCT - Metasys - LIT-12013153 - System Integration - Molex Lighting Integration - 11.0

Metasys System Commissioning for Molex Digital Lighting Systems Integration

Product
Integrations > Molex Lighting Integrations > Molex Lighting Integration
Document number
LIT-12013153
Version
11.0
Revision date
2020-10-30

About this task

After you import both the equipment definition and the controller template, you must create a link between them.

Procedure

  1. Open the controller template in a focus window and select the Configuration tab.
  2. Click Edit.
  3. In the Definition Link parameter, click the browse icon to open the Select Item wizard.
  4. Navigate to the equipment definition and select it.
  5. Click OK.
  6. Click Save.