Inserting the BACnet/IP interface on the network engine - Metasys - LIT-12013153 - System Integration - Molex Lighting Integration - 11.0

Metasys System Commissioning for Molex Digital Lighting Systems Integration

Product
Integrations > Molex Lighting Integrations > Molex Lighting Integration
Document number
LIT-12013153
Version
11.0
Revision date
2020-10-30

About this task

Use the Metasys Site Management Portal (SMP) to commission the network engine. You must have Metasys administrator rights in order to perform the operations detailed in this section.

Procedure

  1. Use the Launcher application to log on to the Metasys SMP UI of the network engine or Site Director.
  2. Drag the network engine device object from the navigation panel to the display panel. The Focus tab screen for the network engine appears.
  3. Click Insert > Integration. The Insert Integration Wizard appears.
  4. In the Select Object Type window, click BACnet IP, and then click Next.
  5. In the Destination window, click the network engine object if not already selected, and then click Next.
  6. In the Identifier window, enter a unique name for the integration, for example, BACnet IP. Click Next.
  7. In the Configure window, you can accept the default settings and click Next.
  8. In the Summary window, click Finish. The Extension Wizard appears.
  9. Click Done.