Network Automation Engine (NAE) - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Product
Integrations > Lighting Integrations > CREE Lighting Integration
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17

An NAE is a web-enabled, IP-based, supervisory engine that connects BAS networks to IP networks and the web. You can use the Launcher application to access the NAE, and then monitor and control BAS devices and systems from a computer. To install the Launcher, use an Internet browser to navigate to the NAE's Site Management Portal. For more information about how to install Launcher, refer to the Metasys Site Management Portal Help (LIT-1201793).

The NAE Series of supervisory engines have various integration capabilities to bring multiple different building system data together to provide smart and powerful outcomes.

All NAEs provide scheduling, alarm and event management, trending, energy management, data exchange, and password protection.

This commissioning guide explains how to integrate a Cree lighting system to an NAE.