Metasys and SmartCast - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Product
Integrations > Lighting Integrations > CREE Lighting Integration
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17

Metasys can monitor and control the SmartCast lighting solution through a BACnet/IP® integration.

Figure 1. Metasys and SmartCast network diagram

Figure 1 shows how the POE or wireless lighting networks communicate with the SmartCast Link device. This device also provides a BACnet server that exposes virtual lighting devices and data points over BACnet/IP. Metasys can integrate this data through an NAE to operate the lighting system using schedules or occupancy logic, or display the lighting system data on Metasys UI dashboards and graphics, and much more.