Introduction - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Brand
Metasys
Product name
CREE Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17
Language
English

This document describes how to commission a Network Automation Engine (NAE) for integration with the Cree® lighting system. In this document, NAE refers to an NAE55, NAE45, NAE35, NCE25, or server-based NAE85, unless noted otherwise.

This document does not describe all the commissioning steps required for a server-based NAE85 to operate on a Metasys® Building Automation System (BAS) network. For more information about commissioning an NAE85 software, refer to the NAE85 Commissioning Guide (LIT-12011044). Also, this document does not describe how to mount, wire, or power on an NAE, and does not describe how to build or download an archive database for a Metasys system site, or how to configure an NAE to monitor and control a BAS.

For information about installing NAE hardware, refer to the NAE55 Installation Instructions (Part No. 24-10051-43), NAE35/45 Installation Instructions (Part No. 24-10050-6), or NCE25 Installation Instructions (Part No. 24-10143-63). For information about installing NAE software, refer to the NxE85 Installation and Upgrade Instructions (LIT-12011530).