About this task
If you are continuing from the Field Device Extension wizard above, proceed to Step 3 with Select Definition Mode.
Procedure
- Drag the lighting device object from the navigation panel to the display panel. The Focus tab for the device appears.
- Click Insert Point wizard appears. . The
- In the Destination window, select the lighting device if not already selected and click Next.
- In the Select Definition Mode window, click Invoke Auto Discovery to begin a BACnet point discovery.
- The Auto Detect Utility wizard appears. This wizard will show that a discovery is in progress. When the new points are discovered from the device, they will appear in the discovery results list. Click Close when the discovery is complete.
- The Point Mapping wizard appears.
Results
Figure 1. Example of light mapped into Metasys