Inserting a field device - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Product
Integrations > Lighting Integrations > CREE Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17

Procedure

  1. Drag the BACnet/IP integration object from the navigation panel to the display panel. The Focus tab for the BACnet/IP integration appears.
  2. Click Insert > Field Device. The Insert Field Device wizard appears.
  3. In the Destination window, select the BACnet/IP integration if not already selected and click Next.
  4. In the Select Definition Mode window, click the Invoke Auto Discovery button to begin a BACnet device discovery.
  5. The Auto Detect Utility wizard appears. This wizard will show that a discovery is in progress. As new BACnet devices are discovered across the network, they will appear in the discovery results list. You should see the Cree lighting devices in this list.
  6. Click the Cree lighting device you want to integrate.
  7. In the Identifier window, enter a unique name for this device. Click Next.
  8. In the Configure window, you can accept the default settings and click Next.
  9. In the Summary window, click Finish. The Extension wizard appears.
  10. Click Done since we are not interested in adding extensions for the device.
  11. The Field Device Extension wizard appears. Click New and continue inserting field points as described below.