Use SCT to create the complete archive - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Brand
Metasys
Product name
CREE Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17
Language
English

Procedure

  1. In the All Items tree, select the NAE for the integration.
  2. On the Facility menu, select Rapid Archive. The Rapid Archive Field Controller wizard appears.
  3. Click Edit.
  4. Click Import, browse to the location of the Rapid Archive Schedule .csv file, then click Import.
  5. After the import completes, the Import Room Schedule dialog appears. Click OK.
    Figure 1. Rapid Archive Field Controller wizard populated with example lighting data

  6. A cell highlighted in red indicates an error. If there is an error, click Cancel, modify the Rapid Archive Schedule to correct the error, and repeat the process from Step 3.
  7. Click Save.
  8. Refresh the All Items tree to verify that your virtual lighting devices and points populated correctly.
    Figure 2. Imported virtual devices shown in All Items tree