About this task
You can download a lighting controller template from the Global Library site: https://globallibrary.azurewebsites.net/#/controllertemplate. The controller template defines a set of points that are available in a lighting virtual device. The controller template is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Controller Templates section in the Metasys SCT Help (LIT-12011964)
For the list of points included in the controller template, see Table 1. The controller template also defines trends for the points. See Table 2.
Item reference | Name | Class ID | Units | States text | Description | Instance number |
---|---|---|---|---|---|---|
BV-1 | Space Occupied | BACnet BV | Unocc / Occ | PIR occupancy sensor | 1 | |
AV-2 | Space Percent Occupied | BACnet AV | % | Percentage of the space that detects occupants | 2 | |
AV-3 | Space Power | BACnet AV | 1/10,000th kW | Real-time power usage | 3 | |
BV-5 | Identify | BACnet BV | False / True | Identify commissioning feature | 5 | |
AV-6 | Light Level | BACnet AV | % | Light level in the Space | 6 | |
AV-7 | Color Temperature | BACnet AV | K | Light color temperature | 7 | |
BV-8 | Lights On Off | BACnet BV | Off / On | Lights on off in the Space | 8 |
Item reference | Name | Class ID | Sample interval | Buffer size | Repository enabled | Client COV increment |
---|---|---|---|---|---|---|
BV-1.Trend1 | Trend - Present Value | JCI Trend Log | 0 | 144 | True | 1.0 |
AV-2.Trend1 | Trend - Present Value | JCI Trend Log | 0 | 144 | True | 10.0 |
AV-3.Trend1 | Trend - Present Value | JCI Trend Log | 0 | 144 | True | 0.01 |
AV-6.Trend1 | Trend - Present Value | JCI Trend Log | 0 | 144 | True | 10.0 |
AV-7.Trend1 | Trend - Present Value | JCI Trend Log | 0 | 144 | True | 10.0 |
AV-8.Trend1 | Trend - Present Value | JCI Trend Log | 0 | 144 | True | 1.0 |
To import the controller template into an SCT archive, complete the following steps:
Procedure
- Download the controller template file from Johnson Controls.
- Launch the SCT, and then open an archive.
- In the All Items tree, expand the Configuration Data folder.
- Right-click the SCT Controller Templates folder, and then click Import Template.
- Navigate to the location of the controller template, select the template, then click Import.
- After the import is complete, a confirmation message appears. Click OK. The controller template imports and is listed under the SCT Controller Templates folder.