Preparing a controller template for lighting in SCT - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Brand
Metasys
Product name
CREE Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17
Language
English

About this task

You can download a lighting controller template from the Global Library site: https://globallibrary.azurewebsites.net/#/controllertemplate. The controller template defines a set of points that are available in a lighting virtual device. The controller template is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Controller Templates section in the Metasys SCT Help (LIT-12011964)

For the list of points included in the controller template, see Table 1. The controller template also defines trends for the points. See Table 2.

Table 1. Point list for lighting controller template
Item reference Name Class ID Units States text Description Instance number
BV-1 Space Occupied BACnet BV   Unocc / Occ PIR occupancy sensor 1
AV-2 Space Percent Occupied BACnet AV %   Percentage of the space that detects occupants 2
AV-3 Space Power BACnet AV 1/10,000th kW   Real-time power usage 3
BV-5 Identify BACnet BV   False / True Identify commissioning feature 5
AV-6 Light Level BACnet AV %   Light level in the Space 6
AV-7 Color Temperature BACnet AV K   Light color temperature 7
BV-8 Lights On Off BACnet BV   Off / On Lights on off in the Space 8
Table 2. Trends for lighting controller template
Item reference Name Class ID Sample interval Buffer size Repository enabled Client COV increment
BV-1.Trend1 Trend - Present Value JCI Trend Log 0 144 True 1.0
AV-2.Trend1 Trend - Present Value JCI Trend Log 0 144 True 10.0
AV-3.Trend1 Trend - Present Value JCI Trend Log 0 144 True 0.01
AV-6.Trend1 Trend - Present Value JCI Trend Log 0 144 True 10.0
AV-7.Trend1 Trend - Present Value JCI Trend Log 0 144 True 10.0
AV-8.Trend1 Trend - Present Value JCI Trend Log 0 144 True 1.0

To import the controller template into an SCT archive, complete the following steps:

Procedure

  1. Download the controller template file from Johnson Controls.
  2. Launch the SCT, and then open an archive.
  3. In the All Items tree, expand the Configuration Data folder.
  4. Right-click the SCT Controller Templates folder, and then click Import Template.
  5. Navigate to the location of the controller template, select the template, then click Import.
  6. After the import is complete, a confirmation message appears. Click OK. The controller template imports and is listed under the SCT Controller Templates folder.

Results

Figure 1. Controller template in SCT