Linking a controller template to an equipment definition in SCT - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Product
Integrations > Lighting Integrations > CREE Lighting Integration
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17

About this task

After you import both the equipment definition and the controller template, you must create a link between them.

Procedure

  1. Open the controller template in a focus window and select the Configuration tab.
  2. Click Edit.
  3. In the Definition Link parameter, click the browse icon to open the Select Item wizard.
  4. Navigate to the equipment definition and select it.
  5. Click OK.
  6. Click Save.