Inserting the BACnet/IP interface on the NAE - Metasys - LIT-12013152 - System Integrations - CREE Lighting Integration - 10.0

Metasys System Commissioning for Cree Digital Lighting Systems Integration

Product
Integrations > Lighting Integrations > CREE Lighting Integration
Document type
Commissioning Guide
Document number
LIT-12013152
Version
10.0
Revision date
2018-12-17

About this task

Use the Metasys Site Management Portal (SMP) to commission the NAE. You must have Metasys administrator rights in order to perform the operations detailed in this section.

Procedure

  1. Use the Launcher application to log on to the Metasys SMP UI of the NAE or Site Director.
  2. Drag the NAE device object from the navigation panel to the display panel. The Focus tab screen for the NAE appears.
  3. Click Insert > Integration. The Insert Integration Wizard appears.
  4. In the Select Object Type window, click BACnet IP, and then click Next.
  5. In the Destination window, click the NAE object if not already selected, and then click Next.
  6. In the Identifier window, enter a unique name for the integration, for example, BACnet IP. Click Next.
  7. In the Configure window, you can accept the default settings and click Next.
  8. In the Summary window, click Finish. The Extension Wizard appears.
  9. Click Done.