Modify - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

About this task

The term modify refers to changing items using the Modify menu item and the Modify dialog box. See the Modify Dialog section.

To edit the attributes of an item:

Procedure

  1. View the details of the item in a display panel.
  2. Select an item tab (for example, Focus).
    Note: Some items contain an Advanced radio button. If you select this button, additional attributes appear.
  3. Click Edit.
  4. Edit the attributes as needed.
    Note: If you place your cursor over an edit field, the ToolTip provides information about the valid format or range for that value. ToolTips also appear for strings.
  5. Click Save.

    For information on using the Modify dialog box to modify single or multiple items, see the Modify Dialog section.