Offline Mode - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

You can use SCT to configure servers and network engines without connecting to the live Metasys server or network engines. This function is called offline, or system configuration, mode. In offline mode, use SCT to set up the system database. Then, load configuration changes created in offline mode to the network engine for the settings to take effect.

Two features are available only with SCT: ActionQ and Manage Archive. You can add servers and network engines in offline mode only.

The offline mode is available to users with the Standard access type. See the Access Types section.