The software can operate in different modes: online using the Site Management Portal UI, and offline using the SCT UI, and Simulation, also using the SCT UI. When you are connected to the network engine or Metasys Server , you can perform online mode operational activities such as monitoring and commanding. When you are connected to the SCT only, you can perform offline mode system configuration tasks such as configuring point objects and features.