Display Panel Tabs - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

Each display panel contains tabs that vary depending on the item displayed.

For example, most of the point objects, such as the OAT contain the following tabs:

Table 1. Tabs

Tab

Description

Alarm

Becomes available when you define an Alarm Extension for a point. The New and Delete buttons allow you to add or delete Alarm Extensions for the point. The Basic and Advanced radio buttons allow you to filter the attribute display in this tab. The Edit button allows you to change configurable attributes.

Focus

Becomes available when you define a point object. The Focus tab shows operation attributes available for the object type to which the object belongs. Note that the Basic and Advanced radio buttons allow you to filter the attribute display in this tab. The Edit button allows you to change configurable attributes.

Hardware

Becomes available when you define a point object that has a reference to a physical input or output. The Hardware tab shows hardware-related attributes available for the object type to which the point object belongs.

BACnet Alarm

Becomes available when you define a BACnet intrinsic alarm for a point. The Intrinsic Alarming Defined attribute is explained in Trend Extension Attributes section. The BACnet Alarm tab shows BACnet Alarm-related attributes available for the object type to which the point object belongs. The Basic and Advanced radio buttons allow you to filter the attribute display in this tab. The Edit button allows you to change configurable attributes.

Totalization

Becomes available when you create a Totalizator Extension. New and Delete buttons allow you to add or delete Totalization Extensions for the point. The Edit button allows you to change configurable attributes.

Trend

Becomes available when you create a Trend Extension for a point object. New and Delete buttons allow you to add or delete Trend Extensions for the point. The Chart view allows you to view data samples in a graphical format and retrieve new trend data. The Table view of the Trend Extension allows you to view the trend’s data samples in a table format. The Definition view of the Trend Extension allows you to view and edit the attributes of the trend extension object.

Averaging

Becomes available when you create an Averaging Extension for a point object. The New button allows you to add Averaging Extensions for the point.

Load

Becomes available when you create a Load Extension for a point object. The New button allows you to add Load Extensions for the point.

Other items may contain fewer or more tabs. For example, the item representing a network engine or Metasys Server contains the following tabs:

  • Focus
  • Summary
  • Diagnostic
  • Communication
  • Network
  • Email (disabled in the ADS/ADX at Release 10.1 and later, but enabled in Metasys UI)
  • Pager (removed from the ADS/ADX at Release 10.1 and later)
  • SNMP (disabled in the ADS/ADX at Release 10.1, but enabled in Metasys UI)
  • Alarm
  • Trend
  • Syslog (disabled in the ADS/ADX at Release 10.1 and later, but enabled in Metasys UI)
  • Printer (disabled in the ADS/ADX at Release 10.1 and later, but enabled in Metasys UI)

For information on the tabs available in the system, see the Object and Feature Tabs section.