Tailored Summary Definition Editor
On a Site Director, the Summary Definition Editor allows you to define and edit an SCT Summary Definition object. The SCT Summary Definition Editor appears when you view an SCT Summary Definition object. In the SMP user interface, you view large quantities of live data in a tabular format. SCT Summary Definition objects always reside on a Site Director in the folder of the All Items tree (that is, you cannot put a SCT Summary Definition object in another location).
Summary Definition Tab
The Summary Definition Editor's Summary Definition tab allows you to define the table that appears in the Tailored Summary Viewer.
|
Button/Field |
Description |
|---|---|
|
Label |
Defines the label to display in the first column (that is, the row header column) in a Tailored Summary. The label is limited to a maximum of 50 characters. This field also can be left blank. |
|
Add/Plus |
Allows you to add a column at the end of the column configuration table. To
select a column, click the column heading.
Note: One column is created by default
when you create the definition. You must define a minimum of at least one
column. The display limitation for Tailored Summaries is 100
rows and 7 columns. You may not see optimal performance when tables exceed
this recommendation.
|
|
Remove/Minus |
Allows you to remove the currently selected column from the column configuration
table. To select a column, click the column’s header.
Note: One column is created
by default when you create the definition. You must define a minimum of at least
one column, and if there is only one column, you cannot delete it.
|
|
Column Configuration Table |
Lets you configure the columns that appear in the Tailored Summary:
Note: To change the order of the columns, select a column and drag it to the
desired placement.
Note: When you display a Tailored Summary, the system searches for data within all
levels of a field device (VMA, for example). For all other objects (NAE, for
example), the system searches for data only one level down (no subsequent
levels).
|
|
Browse (Child Item) |
Opens the Select Item dialog box where you can specify the item name.
Note: This
dialog box provides an easy way to fill in the item name of a child item. It
does not mean that the selected item displays in that column.
|
|
Browse (Attribute) |
Opens the Select Column Attribute dialog box where you can select the attribute to display in the column of the table. This process is necessary only when selecting an attribute other than the default attribute. This dialog box has two list boxes to aid in selection:
Note: To display the default attribute of the row item, leave the Attribute
box set to Default (Attribute Filter: Common Attributes and Attribute: Default).
|
Summary Definition Configuration Tab
|
Attribute |
Description |
|---|---|
|
Name |
Allows you to enter a name for the Summary Definition object. There is a plain text limit of 32 characters. |
|
Description |
Allows you to enter a description of the Summary Definition object. There is a plain text limit of 32 characters. |
|
Object Type |
Indicates the Object Type. |
|
Authorization Category |
Lets you choose the Authorization Category for the Summary Definition object. The default Authorization Category for the Summary Definition object is General. |