Column Attributes for Summary Definitions - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

When creating or editing a Summary Definition, the Select Column Attribute dialog box allows you to select the attributes to display in the Tailored Summary Viewer.

The following table lists examples of the attributes available for display in the Tailored Summary feature according to the attribute filter. Click an attribute in the table to view its description. For information on other attributes that do not appear in this table, search within this Help system PDF by holding down Ctrl + F, or see the Index.

Table 1. Example Column Attributes for Summary Definitions

Attribute Filter

Example Attributes

BACnet

  • BACnet IP Port

  • Instance Number
  • Intrinsic Alarming Defined
  • Object Name

Common Attributes

  • Authorization Category

Field Devices (General)

  • Disable Automatic Alarming

Field Devices (LON)

  • DSN1
  • Neuron ID
  • Program ID
  • XIF Present

Field Devices (MSTP)

  • Memory Usage
  • Object Count
  • Trunk Number

Field Devices (N1)

  • Device Status
  • NCM Name
  • Object Count
  • Poll Delay

Field Points (N2)

  • Controller Type
  • Trunk Number

Field Points (General)

  • Device Type
  • Max Value
  • Min Value
  • Out of Service

Field Points (LON)

  • Command Status Mapping Table
  • Interface Value
  • Target Reference
  • Update Interval

Field Points (N1)

  • Feedback
  • Setpoint

Integrations (MSTP)

  • APDU Retries
  • Buffer Overflow
  • Bus Health Index
  • Bus Performance Index

Integrations (LON)

  • Missed Messages
  • Transmit Errors
  • Transaction Timeouts
  • Transmits Per Minute

Integrations (N2)

  • Command Count

Space

  • Served By
  • Type

Supervisory Devices

  • ADS Repository
  • JCI IP Address
  • Model Name
  • Object Count

Trends

  • Buffer State
  • Enable
  • Sample Interval
  • Transfer Setpoint