Email - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

You can configure email addresses as destinations for event messages. The Email DDA supports standard SMTP. You can also send encrypted email messages.

Note: Beginning at Metasys Release 10.1, configuring the Email DDA in SMP is no longer enabled for the Metasys Server on non-MVE sites, but you can use the Remote Notifications feature in Metasys UI to provide equivalent functionality. Configuring the Email DDA in SMP remains enabled for MVE sites. For details, refer to Metasys UI Help (LIT-12011953).

For information on how to configure an email destination, see Configuring Destination Delivery Agents (DDAs). For information on sending encrypted email messages, see Configuring Encrypted Email.

For additional information, see one of the following sections: