ADS Event Message Forwarding - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

You can forward event messages from one Metasys Server to another Metasys Server on the same site. You also can forward event messages from a Metasys Server on one site to a Metasys Server defined as the Site Director on another site. After forwarding event messages from one site to another, you can configure the Site Director of the receiving site to forward the messages to the other Metasys Server on that site as desired.

See Configuring an ADS Event Repository for information on how to forward event messages from one Metasys Server to another Metasys Server .

Notes:

  • When you forward event messages, the messages are sent (copied) to the ADS repository defined as the Default Destination. The event messages are not removed from the ADS repository that sent the messages.
  • Use message forwarding for notification purposes, not as a backup or archiving method. Use standard SQL practices for backup, archiving, or replication purposes.