Event Enrollment Configuration Example - Signed Out of Range - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The following table is an example of how to configure an Event Enrollment Object using the Signed Out of Range event type. In this example, the Event Enrollment object references the Scale as Integer attribute of an Accumulator Object. An event message is generates as defined by its Event Enable attribute when the value of the ACM’s Scale as Integer attribute goes outside the user-defined low limit/high limit range for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.

Table 1. Signed Out of Range Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Event

Event Message Texts Config

[1]: Scale as Integer is Out of Range

Input Reference

ACM1

Scale as Integer

Delay Time (seconds)

120

Event

Low Limit

-2

High Limit

7

Deadband

5