Event Enrollment Configuration Example - Out of Range - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The following table is an example of how to configure an Event Enrollment Object using the Out of Range event type. In this example, the Event Enrollment object references the Present Value attribute of an Analog Input Object. An event message is generated as defined by its Event Enable attribute when the value of the AI’s Present Value attribute goes outside the user-defined low limit/high limit range for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.

Table 1. Floating Limit Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Event

Event Message Texts Config

[1]: Room Temp Out of Range

Input Reference

AI1

Present Value

Delay Time (seconds)

300

Event

Low Limit

66.0

High Limit

74.0

Deadband

2.0