Event Enrollment Configuration Example - Command Failure - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The following table is an example of how to configure an Event Enrollment Object using the Command Failure event type. In this example, the Event Enrollment object references the Present Value attribute of a Binary Input Object. An alarm message is generated as defined by its Event Enable attribute when a command to SA_F’s Present Value attribute is not reflected by the Input Reference (SA_FLOW) after the defined Delay Time has expired. For more information about this event type, see Event Type.

Table 1. Change in Command Failure Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Alarm

Event Message Texts Config

[1]: Supply Fan Command Failure

Input Reference

SA_FLOW

Present Value

Delay Time (seconds)

60

Event

Command Target

SA_F

Present Value