Event Enrollment Configuration Example - Change of State - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The following table is an example of how to configure an Event Enrollment Object using the Change of State event type. In this example, the Event Enrollment object references the Reliability attribute of a Multistate Value Object. An Event message is generated as defined by its Event Enable attribute when the state of the MV’s Reliability attribute changes to Unreliable for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.

Table 1. Change of State Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Event

Event Message Texts Config

[1]: Point is now Unreliable

Input Reference

MV1

Reliability

Delay Time (seconds)

0

Event

Event Type

Change of state

Value

Unreliable