Event Enrollment Configuration Example - Change of Character String - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The following table is an example of how to configure an Event Enrollment Object using the Change of Character String event type. In this example, the Event Enrollment object references the Present Value attribute of a Character String object. An event message is generated as defined by its Event Enable attribute when the Character String's Present Value attribute partially matches one of the List of Values for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.

Table 1. Change in Character String Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Event

Event Message Texts Config

[1]: Change in Object String Detected

Input Reference

CharString1

Present Value

Delay Time (seconds)

120

Event

List of Values

Security Breach

Power Failure