Event Enrollment Configuration Example - Change of Bitstring - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The following table is an example of how to configure an Event Enrollment Object using the Change of Bitstring event type. In this example, the Event Enrollment object references Status flags of an Analog Value Object. An event message is generated as defined by its Event Enable attribute when either the In Alarm or Fault attribute changes to True for a time period longer than the defined Delay Time. For more information about this event type, see Event Type.

Table 1. Change in Bitstring Example

Tab

Attribute

Value

Focus

Event Enable

To Off Normal

Notify Type

Event

Event Message Texts Config

[1]: Change in Status Detected

Input Reference

AV1

Status Flags

Delay Time (seconds)

10

Event

Mask

In Alarm - selected (true)

Fault - selected (true)

Overridden - not selected (false)

Out of Service - not selected (false)

Values

In Alarm - selected (true)

Fault - selected (true)

Overridden - not selected (false)

Out of Service - not selected (false)