Enabling Advanced Auditing - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

About this task

The Equipment Activity widget captures audits of commands performed by Schedule objects, Multiple Command objects, and Interlock objects that are tied to equipment configured to the Metasys UI. To use this feature, you must make sure that the Engine object is at Metasys Release 8.0 or later and the Enable Application Generated Audits attribute is set to True.

Procedure

  1. In SMP, open the Engine object's Focus tab.
  2. Select Advanced.
  3. Click Edit.
  4. Under the Audit Trail section, change the Enable Application Generated Audits value to True.
  5. Click Save .