The following table describes the two types of audit repositories for storing audit messages in the Metasys system. The ADS Audit Repository applies to either Metasys Server: ADS or ADX.
|
Type |
Description |
|---|---|
|
Local (Engine) Audit Repository |
|
|
ADS Audit Repository |
|
For information on configuring the Engine local audit repository and the default destination, click one of the following:
A Database Timeout Error can occur when viewing audit messages if the repository contains too many unfiltered audit messages before the system times out (typically, one million messages). To prevent this error, back up and purge audit message records from the repository (JCIAuditTrails) using the Metasys Database Manager on a regular basis.