Enable Alarm Pop-Ups - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Menu Selection: View > Enable Alarm Pop-Ups (select the check box to enable/disable alarm pop-ups)

For the current user session, this item determines if the pop-up Alarms Window (also referred to as Metasys - Events or Alarm Bar) automatically displays when an alarm is detected.

Clicking the alarm icon in the status bar re-enables alarm pop-ups and displays the current alarm, if any.

If you disable the alarm pop-up window and you have the audible alarm option enabled, the audible alarm sounds when an alarm is detected. See the Alarms Window section in the Site Management Portal User Interface.