Creating a Repeating Monthly Report - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

About this task

To create a repeating monthly report that runs on the 15th and last day of every month at 8:00 A.M. with no end date:

Procedure

  1. Repeat step 1 to step 4 in Creating a Daily Report.
  2. Select Run This Report Monthly.
  3. Verify the Start Date is set to today.
  4. Select the No End Date check box.
  5. In the Date Information section, select 15 and Last (Ctrl + click).
  6. In the Time Information section, configure the Run At time information to 8:00 A.M.
  7. Click Save.