Menu Selection:
Inserts a supervisory device into the archive database with SCT.
Metasys System: NAE35, NIE39, NAE45, NAE451L, NIE49, NAE55, NIE59, NAE85, NIE89, NCE25, NIE29, NIE55, NIE85, SNE10/SNE11/SNE22, and SNC16/SNC25. You can insert a device at a previous Metasys system release with SCT, beginning with Release 5.2 and later. The SNE and SNC devices are only available to SMP at Release 10.1 or later, and SCT Release 13.2 and later.
FX System: SNC16 and SNC25.
Note: The Metasys NAE451L and SNE110Lx
network engines are available only to select regions of Australia, China, Hong Kong, India,
Indonesia, Japan, Korea, Malaysia, New Zealand, Philippines, Singapore, Taiwan, Thailand,
Vietnam, and select branches.
On the Configure screen of this wizard, click any tabs that may appear for further device configuration.