Summary Definition Attributes - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. For information on the Tailored Summary feature, see the Tailored Summaries section in the SCT: System Configuration Tool Help (LIT-12011964) .

Click the attribute name in the table for a description of the attribute.

Note: In the notes column, attributes marked with the letter C are configurable, attributes marked with the letter N do not require a value, and attributes marked with the letter W are writable.
Table 1. Summary Definition Object Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Key Data

C,N,W

 

Limit of 4 key items

Holds the item name or Fully Qualified Reference of a key item to display in a tailored summary. You can configure up to four key items.

Table 2. Summary Definition Object Attributes - Summary Definition Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Column Definition

C,W

 

Column Heading, Child Item, Attribute

Defines the columns displayed in a tailored summary. You can define up to seven columns (list of structures).

Each structure contains the following information:

Column Heading - Defines the name of the column header.

Child Item - Indicates item for which the column data is retrieved based on its name attribute, which must match a user-specified pattern (such as ZN-* or ZN-T, Zone-T). To display an attribute of the row item, leave this field blank. Otherwise, specify the name of the child item to display.

Attribute - Defines the attribute information for the column. The attributes are grouped into categories for easy selection. Select a category in the Attribute Filter section of the Select Column Attribute dialog, and then select the desired attribute from the list.

Row Heading Column Text

C,N,W

 

Label

Maximum: 50 characters

Defines the text to display as the label for the row headings column (that is, the first column) in a tailored summary.