Program Attributes - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Note: In the notes column, attributes marked with the letter C are configurable, and attributes marked with the letter W are writable. For more information about attribute characteristics, see Attributes.
Table 1. Program Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description of Halt

     

Enabled

C,W

   

Instance Of

     

Program Change

W

Ready

0 = Ready

1 = Load

2 = Run

3 = Halt

4 = Restart

5 = Unload

Program Location

     

Program State

   

0 = Idle

1 = Loading

2 = Running

3 = Waiting

4 = Halted

5 = Unloading

Reason for Halt

   

0 = Normal

1 = Load Failed

2 = Internal

3 = Program

4 = Other

Reliability

   

Uses Reliability set.