Editing Bool Blocks - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

About this task

Note: LTCH (Latch) blocks are not editable.

To edit Bool blocks in Edit mode:

Procedure

  1. Double-click a Bool block. The configuration dialog box appears.
  2. Edit the fields and configure the number of inputs based on the selected type of Boolean logic.
    Table 1. Bool Block Configuration

    Field

    Description

    Input

    The number of inputs depends on the type of Bool block you use. You cannot reduce the input count lower than the number of current connections.

    OK

    Accepts changes.

    Cancel

    Cancels changes.