Editing Attribute Reference Inputs - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English
Table 1. Attribute Reference Input

Field

Description

Label

Enter a label here for the block.
Note: Do not start labels with a number and then follow it with any of these characters: $ . - ,

Object

Browses to the object to which the reference is linked. Leaving this field blank leaves a placeholder for a future reference. The dragged object's name appears in this field and the object's attributes appear in the drop-down list in the attribute field.

Attribute

The attribute to which the reference is linked. When you are configuring for an Input reference, the drop-down list contains numeric attributes only.

Units

Units for the attribute

Trigger

This is checked if you want the attribute to trigger the control system to execute immediately instead of waiting for the next control system scan if the value changes by more than the defined increment. Otherwise, the control system executes normally.

Increment

Sets the increment.

OK

Accepts changes.

Cancel

Cancels changes.