TMR (Timer) - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

This table describes the components of the TMR blocks:

Table 1. TMR (Timer) Blocks

Output

Description

IN

Input

RS

Reset. Cancels the timer. Reset does not apply to Minimum On or Minimum Off timers. Use a binary object attribute for Reset (1.0=Reset Active, 0.0=Reset Inactive).

The LCT contains five different types of timers. Each type uses a Duration (how long the timer is active) and unique functions to generate an Output. The different types of timers are listed below. Click the name of the timer for a description and figure of timer operation.

For information on setting Duration and the type of Timer, see Editing Timing Blocks.