The following table and figures illustrate the function of the On Delay timer.
|
Feature |
Description |
|---|---|
|
Activation |
Goes inactive in a low to high Input transition, depending on the state of the input during the duration period. If the Input returns to a low state (inactive), the timing cycle is canceled and the Output remains inactive. If the Input remains in a high state, the Output goes to the high state at the next execution of logic. In a high to low Input transition, the Output becomes inactive the next time the logic executes (logic executes every 5 seconds). |
|
Output |
See row above. |
|
Reset |
Cancels timer activity and makes the output inactive. If the Reset goes from active to inactive, the timer re-evaluates the Input at the next low to high transition. |
|
Example |
Delays the supply fan start 20 seconds after the return fan starts. |