Statistical Category - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Statistical blocks perform statistics on input. The number of inputs to a Statistical logic block depends on the number of inputs supported by the type of statistic. The Logic Connector Tool allows you to add multiple connections to the output of the block.

Table 1. Statistical Block Connections

Statistical Type

Inputs

AVG

2–8

MAX

2–8

MIN

2–8

See Editing Blocks in Edit Mode for information on editing Statistical blocks.