Control Category - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Most control logic blocks have three inputs, and you can add multiple connections to the output of the block. The blocks compare input number 1 with input number 2 using the differential (input number 3). The type of control depends on the statistical type. The Sequencer functions differently. See SEQ (Sequencer) for details.

Table 1. Control Blocks

Block

Statistical Type

Inputs

X>Y

greater than

3

X<Y

less than

3

X<=Y

less than or equal

3

X>=Y

greater than or equal

3

<>

not equal

3

=

equal

3

SEQ

Sequencer

See SEQ (Sequencer) for details.

See Editing Blocks in Edit Mode for information on editing Compare blocks.