Bool blocks apply Boolean functions to input. The number of inputs to a Bool logic block depends on the number of inputs supported by the type of Boolean function. The Logic Connector Tool allows you to add multiple connections to the output of the block.
|
Bool Type |
Inputs |
|---|---|
|
AND |
2–8 |
|
OR |
2–8 |
|
XOR |
2 |
|
NOT |
1 |
|
LTCH |
See LTCH (Latch) for details. |
See Editing Blocks in Edit Mode for information on editing Bool blocks.