Logic Checker - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The Logic Checker is not the same logic check run with a LCT save. It must be selected from the Toolbar. The Logic Checker scans the control system logic and reports any configuration issues it finds.

Table 1. Logic Checker

Condition

Message Text

Message Text Position

An output is not connected.

Missing Output Connection

Top-center of the block

An input is not connected.

Missing Input Connection

Top-center of the block

A feedback loop exists in the logic.

Feedback Loop Is Present

Top-center of a connection in the loop

An attribute is not connected.

Attribute Is Not Connected

Top-center of the attribute

Duplicate attribute name is defined.

Duplicate Attribute Name

Top-center of the attribute