Connections - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Connection lines connect blocks in the logic. The LCT does not do a datatype check; that is, you can connect Boolean and Constant values, and any other combination. But, the tool does not allow inputs to connect to inputs, or outputs to outputs. The tool determines the connection line routing, and the only way to change the routing is to move the blocks or use the hide feature.